Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Safe - Pre-Loaded SNAP IN Connection Guarantees Safe Connection of the Conductor

SNAP IN terminals are “ready to wire” as the conductor is terminated in the pre-loaded contact and no preparation or tool is required. Connections are always Safe because the wire is only contacted if inserted properly into the contact point. A safe contact is indicated visually with a raised pusher and with an audible click.

PTM Veröffentlicht am: