Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
REDFIT-Slide10

The main characteristics of the techincal data are: that the VIA is fully specified on the right side below the pinout. This is important because the VIA acts like the mating partner. With this data, it is possible for the PCB manufactuer to manufacture the correct VIA. The restring has to be as small as possible for SKEDD technology, as it is not necessary and there is no soldering. This is also done to meet the clearance and creepage distance needs.

PTM Veröffentlicht am: