Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Image of Würth Elektronik Thermal Interface Materials - TIM

Thermal interface materials are what makes sure that the thermal transfer between the heat source and the cooling assembly is as efficient as possible. Even though the contact surfaces of the heat source and the cooling assembly seem flat and coplanar, microscopic irregularities have a huge toll on the thermal performance of the system. Thermal interface materials make sure that there are no gaps between the heat source and the cooling assembly and provide a low thermal resistance path for heat to flow through.

PTM Veröffentlicht am: