Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Signal Transmission Through a Capacitive Isolation Barrier

Digital isolators transfer signals across an isolation barrier. This is achieved by using a modulator to transmit high-frequency signals through the barrier. The receiver demodulates the high-frequency signal into an output signal mimicking the input signal. There is always a delay between the input signal arriving to the input channel and the output signal leaving the output channel. For high-speed applications, it is very important to have this delay as small as possible, which is an area capacitive digital isolators excel at due to their lightning-fast delay times.

PTM Veröffentlicht am: