Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Spartan 3 Generation FPGAs Slide 6
The Spartan series integrates hard IP blocks for easy implementation and improved resource utilization, resulting in lower total system cost. The extended Spartan-3A family has DSP48A blocks to improve the complex computation capability of the standard Multiplier/Logic Cell implementation. Real function benchmarking shows a 50 to 1300 logic cell savings by utilizing the DSP48A block. Results also show, an average savings of 300 logic cells or 70% improvement in density by utilizing the DSP48A in the Spartan devices.
PTM Veröffentlicht am: