Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Laminating-Slide3

Acrylic adhesives are specifically formulated to meet the most demanding applications in the electronics market. They provide high temperature holding strength, excellent chemical and solvent resistance and high tensile strength. There are two application groupings commonly used in the electronics industry, high surface energy & harsh environments, and low surface energy & challenging surfaces.

PTM Veröffentlicht am: