Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Laminating-Slide4

For the first application grouping, high surface energy and harsh environments, the 3M adhesive 200MP and 100MP families should be considered. In the graphic above, the y-axis represents temperature, solvent and shear performance whereas the x-axis represents typical adhesion levels. The temperature shown above is from 200 deg F to 500 deg F on the y-axis. The typical adhesion level is 181 oz/inch to stainless steel represented on the x-axis.

PTM Veröffentlicht am: