Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
heatsink-attachements-slide13

Next, place the heat sink squarely over the component, ensuring that the fins are lined up according to the direction of the airflow in a system. Secure the “open end” of the spring clip under the top of the frame clip. Using the “forked” end of the spring clip tool, latch over the “closed end” of the spring clip on to the frame clip tab. Finally, inspect the installation and make sure the heat sink is securely attached. 

PTM Veröffentlicht am: