Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
heatsink-attachements-slide5

Extensive CFD analysis and experimental testing has been performed to study the thermal impact of the frame-clip and spring clip in the maxiGRIP assembly. These studies have shown that the low profile of the frame clip and the minimal cross-sectional area of the spring clip allow for maximum airflow through the heat sink and hence maximum cooling power. 

PTM Veröffentlicht am: