Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
NTC-Slide2

NTC Thermistor Sensors are temperature-sensing elements made of sintered metal oxide that display large changes in resistance in proportion to small changes in temperature. This resistance is measured by using a small and measured direct current passed through the thermistor in order to measure the voltage drop produced. These solid state temperature sensors actually act like electrical resistors that are temperature sensitive. That is where the name thermistor, a clear combination of the words thermal and resistor, comes from.

PTM Veröffentlicht am: