Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
ZipLine Connector System Slide 15
This slide shows two items of interest. First, it highlights the different tail patterns for standard backplane and orthogonal midplane header configurations. It also demonstrates that IMLAs can be selectively loaded into the housing, in these examples spacing adjacent columns on 3.6mm centers. Wider column spacing may be desirable in designs where trace routing and PCB layer count are concerns, and density is not.
PTM Veröffentlicht am: