Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
ZipLine Connector System Slide 9
FCI ZipLine™ signal connector modules include 6 pair connectors in both 12 and 16 column variations on 1.8mm centers. In addition to traditional backplane configurations, some customers have asked for an orthogonal interface between opposite sides of a midplane. FCI has responded with a header that facilitates this type of interconnect. Note that the ZipLine right-angle receptacle module can be used in both backplane and orthogonal midplane applications.
PTM Veröffentlicht am: