Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
AFI-Slide2

The AFI interface was developed to achieve a higher level of density in a crash-proof, blind mate connector system. It was designed to be superior to other product currently on the market. This is a drastic improvement over existing blind mate systems which can crash if their float capabilities are exceeded. The Amphenol AFI has built in protection to eliminate damage from mating, or from production test fixtures.

PTM Veröffentlicht am: