Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
HD-BNC 50 Ohm Slide 15
In summary, there are several reasons why users should consider using a 50 HD-BNC™ in their next project. The same trusted bayonet style, locking and visual indicator are used on the HD-BNC™, eliminating assembler training. It provides an avenue to save space and equipment weight with its 51% smaller foot print. The product’s VSWR or return loss of 30dB min@ 6GHz is excellent. Amphenol offers a full product portfolio, which also includes adapters and a calibration kit.
PTM Veröffentlicht am: