Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
atmosphere-slide12

Once a project is ready to be tested, it can be “built.” Building is a process in Atmosphere Developer that compiles the project in the Atmosphere cloud server, and allows it to be accessed by the rest of the Atmosphere development suite. It is also what simultaneously creates the project’s embedded system firmware and the mobile app’s software. After the project is built, the Anaren MSDK’s A20737 module has to be programmed with the firmware.

PTM Veröffentlicht am: