Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
atmosphere-slide15

From there, all that is left is to connect to the MSDK. The Atmosphere app can scan for Bluetooth-enabled devices in the area and connect to them. So scan for and connect to the Anaren MSDK via BLE, and the app is then paired to the device. Once connected, the app can interact with the MSDK based on the project’s functionality. It is that simple to build a project and enable it for IoT connectivity using Anaren Atmosphere.

PTM Veröffentlicht am: