Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
imp feat
The LDS series has numerous important features and benefits. The supplies can support system life requirements greater than fifty thousand hours, no forced air is necessary for cooling and both models have no minimum load requirement. Active power factor correction rated at 0.9 typical minimizes input harmonic current distortion. In addition, current levels can be preset by the system designer or adjusted in application to perform dimming functions.
PTM Veröffentlicht am: