Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Image of Artesyn Embedded Technologies LGA50D Non-Isolated DC/DC Converter-Slide5

The applications that can be addressed are wide and varied. The LGA50D is suitable to be used with highly power-rated devices such as server processors and FPGA’s, but is also suited to be used with panels of LED’s. This means that the unit can be used in applications such as graphics, data or video processing as well as supercomputers, network, storage and telecommunication equipment.

PTM Veröffentlicht am: