Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Image of Artesyn Embedded Technologies LGA50D Non-Isolated DC/DC Converter-Slide6

To evaluate the LGA50D, Artesyn also provides an evaluation kit. The kit contains a PCB with 2 of the LGA50D’s and some external components mounted on to it to allow the user to connect to the LGA50D either via the PMBus interface with the interconnect cable and dongle provided. However, if hardware configuration is preferred, the user can select the configuration of the modules by setting the DIP switches that are mounted on the evaluation card and enable the operation of the unit with the toggle switch provided. There are also voltage and current monitoring connections provided for the user to directly connect to.

PTM Veröffentlicht am: