Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
SAMA5D3-Slide16
Not all customers necessarily need to use an OS or RTOS.  More specifically, when it comes to a quick evaluation of the processor functionalities or a quick test on a new hardware (PCB board), designers do not want to spend time implementing a heavy OS; this is where the Microchip software package comes into play. It offers around forty examples in C/C++ that exercise most of the SAMA5D3 features. Finally, Microchip delivers a full package to customers interested in implementing a secure boot solution. This includes a generic presentation, multiple application notes, and PC software. The secure boot package is delivered under restricted conditions and requires an NDA; contact an Microchip sales facility.
PTM Veröffentlicht am: