Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
SAMA5D3-Slide7

Having three high-speed USB ports is unique and offers significant advantages over the USB OTG peripherals that can be found on the market. Considering the growing need for connectivity, users can connect a Wi-Fi/BT module on one port while keeping two others for a mouse or keyboard, and a USB key. As a reminder, high-speed (HS) USB 2.0 has a maximum theoretical speed of 480 Mbit/sec., whereas full-speed (FS) USB 2.0 has a maximum theoretical speed of 12Mbit/sec. All SAMA5D3 USB ports have an integrated transceiver. No external PHYs are required. The SAMA5D3 is different than the SAM9x5 series; the SAMA5D3 features three HS Hosts, the SAM9x5 offers two HS Hosts and one FS Host. 

PTM Veröffentlicht am: