Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
AMS22U-Slide5
The Bourns® AMS22U position sensor with ball bearings has excellent performance over life. This is very important in applications where the cost of replacing the sensor is high, as well as applications where the sensor is in a remote location and access for repair and replacement is limited. As compared to contacting technologies, this position sensor provides extremely long life and reliability, reducing the cost of repair and maintenance.
PTM Veröffentlicht am: