Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
leds for low light

A light-emitting diode (LED) is a semiconductor device that emits narrow-spectrum light when electrically biased in the forward direction of the PN junction. This effect is a form of electroluminescence. LED displays use more power (up to 200mA) but produce more light per watt than do incandescent bulbs and work well in low light applications, which is useful in battery powered or energy-saving devices. LEDs also have the best viewing angle and can be read from virtually anywhere in the room. When environmental conditions exist, the LED’s response time is not visibly affected (“ghosting”) even at temperatures below -20 degrees Celsius.

PTM Veröffentlicht am: