Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Product List
CameraLink-Cable-Slide6

In summary, Cicoil's Highly Flexible Flexx-Sil™ Jacketed Camera Link® cables were created to meet the increased demand of industrial motion video, vision systems and frame grabber application requirements. Because the conductor spacing is fixed and the geometry of the cable is constant, the electrical characteristics, such as impedance, capacitance, inductance, time delay, crosstalk and attenuation, are consistent. All wires are fully encapsulated in ‘glass-clear’ Flexx-Sil™, a solid, one-piece construction that creates a highly durable cable package. The cable will not deform, break or wear for the lifetime of the product, even in high flex applications.

PTM Veröffentlicht am: