Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
SPD-Slide11

Placing the ESD diode as close to the input source as possible ensures most of the surge is diverted through the protection devices. Having the shortest trace to the ESD diodes also helps lower the resistance, and channels the surge energy through the ESD diodes instead of the device being protected. Connecting the ESD diodes to the chassis ground or reference ground instead of signal ground is preferable and makes the layout more robust.

PTM Veröffentlicht am: