Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide17

Shown here this slide gives a quick cross reference for comparing XP-G2 to the original XP-G in outdoor white. This allows one to easily compare the performance of the two products at two different binning temperatures. Using the example at the bottom of the page, an XP-G2 from the R3 Flux bin which delivers a minimum of 122 lm at 350 mA and 85°C has similar light output compared with an XP-G R5 flux bin which delivers a minimum of 139 lm at 350 mA and 25°C. It is important to utilize this cross reference when making initial comparisons as flux at different binning temperatures are very different. Please note that this is just a guide. For a more accurate comparison between Cree products, Cree recommends using the Product Characterization Tool (PCT) available at Cree.com.

PTM Veröffentlicht am: