Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Rocker-Slide13

Maintained-contact switch configurations are: ON/OFF, ON/ON, and ON/OFF/ON. Momentary rocker switches have the following switch functions: Momentary ON (NO), Momentary OFF (NC), and three position momentary center-OFF. Momentary ON describes contacts which interrupt the circuit when the rocker switch is in the normally open (NO) position, momentary OFF describes contacts which establish a circuit when the rocker switch is in the normally closed (NC) position.

PTM Veröffentlicht am: