Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Rocker-Slide5

The CW 4000 Series product offering is presented in the chart shown on this slide. To identify the right series for an application, the user must determine the following: the switch function, maintained, momentary or center off; the electrical rating required, 8A, 13A or 16A; and the circuitry for the application, SPST, SPDT, DPST, or DPDT. As an example, a GRS 4011-13 is a maintained action, single pole, single throw miniature rocker rated at up to 13A.

PTM Veröffentlicht am: