Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
CliQ and CliQ II Series: DIN Rail Power Supplies Slide 15

The CliQ series models designed for 3 phase input voltage, can start up at a very low input voltage and do not require any power de-rating across entire input voltage range from 320 to 575 VAC. The advantage of CliQ’s 3 Phase input is that during a loss of one input phase, the unit is still able to deliver 100% output power at a minimum input voltage 360 VAC. Competitor A can only start up at relatively higher input voltage for 3 phase input and can only support a lower load when one phase is lost. Competitor D has power de-rating of 75% rated load during the loss of one phase and is much more expensive.

PTM Veröffentlicht am: