Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Common-Circuit-Slide13

Mistakes often occur when specifying the degree of protection. Terms such as drip-proof, ignition protection, water splash protection, and dust-proof are all common usage, but may be misleading unless standard defintions are applied. When specifying, use the established standards as a measure, such as DIN EN 60529/IEC 529, which defines degree of protection of electrical equipment. Using these standards, decide which protection is correct for the application.

PTM Veröffentlicht am: