Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Common-Circuit-Slide9

The second common mistake is specifying to avoid nuisance tripping. Most engineers are concerned about nuisance tripping, as they should be, but they often specify a circuit breaker rated  much higher than they should. Part of the reason is confusion between fuses and circuit breakers. Engineers are used to oversizing fuses as a way to prevent nuisance tripping. However, there is no need to oversize a circuit breaker.

PTM Veröffentlicht am: