Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
conversion-slide6

A buck converter is a step-down DC to DC converter. Today, converting from a common 48V power bus down to voltages around 1V requires two stages due to the switching limitations of power MOSFETs. Direct conversion from 48V to low voltage could eliminate the cost and space of a two stage solution if the overall efficiency of the system can be maintained.

PTM Veröffentlicht am: