Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
second-Gen-Slide14

In addition to a higher pulsed current rating and less conduction  loss at higher current, the new generation EPC2012 has improved RDS(ON) at lower gate-source voltages. This results in allowing the user to realize the low RDS(ON) capability of the FETs with greater margin between the applied gate voltage and the VGS(MAX) of 6V.

PTM Veröffentlicht am: