Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
second-Gen-Slide3

These four figures compare the 100V, 25A EPC2001 (Figure 1) with the prior-generation EPC1001 (Figure 2) typical output and transfer characteristics. The left figures show that the new generation product performs significantly better at higher currents. The right figures show that VGS necessary for significant conduction current has also increased, thereby reducing turn off time and increasing dv/dt immunity.

PTM Veröffentlicht am: