Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
VLISI-Slide7

Several of the processors are now requiring a ratio-metric voltage matrix implementation with a guard band. Stated slightly differently, this means that the processor measures its environment; die temperature, clock speed, die voltages and the level of system utilization, and then dynamically changes the core voltage and memory voltage as needed. As can be seen in the chart on this slide, as the core voltage is modulated the memory voltage is also controlled within this guard band. This is specified to optimize the system performance per watt of utilization. Notice the degree of accuracy and resolution necessary to make this work properly, precision is assumed in this application.

PTM Veröffentlicht am: