Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
advantages
At 12Mbps, the XR21V141x are some of the industry’s fastest UARTs. MaxLinear's USB UARTs are some of the industry’s smallest package 1-ch, 2-ch and 4-ch USB UARTs. They offer several features which translate into an overall cost effective solution. A standard CDC-ACM driver can be used to run these USB UARTs. In addition, a custom driver is also available. On-chip features such as the fractional baud rate generator allow for any baud rate up to 12Mbps to be generated.
PTM Veröffentlicht am: