Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Advanced Energy Xgen Configurable Power Supplies - Slide10

This page shows an example of the Advanced Energy power supply Configurator Wizard that is available on the DigiKey web site. Simply enter each combination of voltage and amperage, and the Configurator will provide a complete solution. The Configurator then provides a table which lays out which output modules are needed. It also provides a complete part number.  All outputs are floating and fully isolated, so you may enter negative and positive voltages.

PTM Veröffentlicht am: