Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Flexis QE Series Low Power Features Slide 6
The Flexis series of QE 8-bit and 32-bit microcontrollers are the industry’s first 8- and 32-bit microcontrollers with pin-for-pin compatibility and a common set of both on-chip peripherals and development tools. The unprecedented compatibility is only one unique feature of the QE128. Additionally, the QE128 devices are the first to host NXP’s ultra-low power features and benefits.
PTM Veröffentlicht am: