Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
ft800 graphics engine widget2
The graphics commands are sent to the command buffer in a similar fashion as the Display List used for primitives.  Display List commands can also be embedded into the Graphics Engine command list.  The command list in this slide would perform the same function of blanking the display as the initial Display List in slide 16. As with sending data for the Display List, these commands indicate to send certain bytes over the SPI or I2C interface to a particular memory location.  For the example Command List shown in the first list above, the actual data that is written over the interface is in the second list.
PTM Veröffentlicht am: