Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
designing with hard2
The FT800 supports a re-ordering, or “swizzling”, of the data LCD RGB data bits pin assignments. This allows a direct PCB layout from the FT800 to the LCD connector.  In addition to swizzling, the display data clocked on the RGB pins can be spread so that all 18 bits are not changing at the same time. Both the swizzling and spread data help to positively impact electromagnetic effects.
PTM Veröffentlicht am: