Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
write on off settings
Next to be covered is how to turn the module on and off. Click on the button next to the on/off options and four menu items will appear: Always on, Analog on, Digital on, and Analog or Digital on. The default is analog on which allows the module to be controlled using an external enable signal. Now change this to Digital on. Notice that the “On” checkbox at the top of the settings list is not checked, but the module is still running. This is because the new configuration still needs to be written to the module, which is done by clicking the “Write Settings” button.
PTM Veröffentlicht am: