Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Digital-Slide18

This slide shows an example of how digital control can be used to improve total system performance. In this case, a digital Barracuda bus converter is used to convert 48V down to a bus voltage that is then used to power several DLynx POLs down the line. The classic question in this case is “what is the best bus voltage”? The Barracuda Bus is capable of reading the bus current and setting the bus voltage, allowing for a range of potential answers.

PTM Veröffentlicht am: