Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Human Interface Applications

Encoders designed for human interface applications are often available with a pushbutton feature incorporated into the shaft. After the cursor is moved to the desired menu item, the operator pushes the shaft to “enter” that choice. This is similar to the “clicking” function on a mouse. In this example the operator chooses menu item “F” and “drills down" to an additional submenu.

PTM Veröffentlicht am: