Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Optical Encoder Slide 6

This output code is called “Quadrature” because it repeats itself every four positions. It can also be shown in a “Truth Table”. Quadrature encoders are also called INCREMENTAL encoders. A microprocessor chip that reads a quadrature encoder can only determine the direction, clockwise or counterclockwise, and the amount of increments, that the encoder shaft has been rotated. A microprocessor cannot determine the absolute rotational position of the shaft. This is because the output code is exactly the same in different positions. For example, in positions 1,5,9 and 13 as shown in the Truth Table.

PTM Veröffentlicht am: