Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
thermstrate
Thermstrate is one of the first PCTIMs developed in the 90s. This material features a thermally conductive phase change material coated on aluminium substrate. The material melts at 60°C, providing excellent wetting and heat dissipation. Note that this material is not electrically insulating.
PTM Veröffentlicht am:
PTM Updated on: 2017-06-14