Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
pctim contd
The advantage of PCTIM is that it offers 100% wetting at the interface and virtually zero interfacial thermal resistance. As the compound goes from solid to liquid, it expands 16% in volume. This forces out entrapped air and eliminates voiding. The material shrinks back to the interface when it cools, preventing pump-out.
PTM Veröffentlicht am:
PTM Updated on: 2017-06-14