Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Ha-VIS preLink - Ethernet Cabling System Slide 4

Step 2: The termination block is inserted into the Ha-VIS preLink® crimping tool. With a single operation of the crimping tool, the IDC contacts in the termination block engage the copper wire, while at the same time the excess wire is trimmed from the end of the termination block. The HARTING preLink crimping tool ensures that the wires are assembled correctly 100% of the time.

PTM Veröffentlicht am: