Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
har-flexicon-slide10

The 1.27 mm version utilizes an IDC termination design for use with stranded wires. Termination is achieved by inserting each of the four single wires into the wire manager. Once inserted the wires are pushed to the end stop to ensure correct positioning. Then the wire manager can be closed, allowing the IDC blades to terminate to the wire. No special tooling is required.

PTM Veröffentlicht am: