Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Improved, Robust Product Range

The choice of a 1.27 mm (0.05”) pitch connector as an alternative to 2.54 mm (0.1”) pitch connector saves space and weight on the PCB. Many applications do not require the current carrying load of the larger pitch, and the 50% space saving frees up a significant amount of space for other components or smaller units overall. However, the demand for more robust electronics suitable for industrial markets is increasing. Connectors originally designed for consumer electronics now need to withstand the additional demands of the factory floor.

PTM Veröffentlicht am:
PTM Updated on: 2025-06-16