Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF59S-SN-Slide2

The DF59S/DF59SN series is a slim fit, low profile mono-pole connector, optimized for LED lighting applications. In addition to DF59S that has a 2.7mm depth, the super slim DF59SN has a depth of 1.7mm. The unique “Stress free contact” has a floating function of ±0.5mm in the X and Y directions and ±0.2mm in the Z direction.

PTM Veröffentlicht am: